cancel
Showing results for 
Search instead for 
Did you mean: 

DiscoF4 - is R31 populated on RevE or not?

waclawek.jan
Super User

Schematics say, it is populated on Rev.B and Rev.E,  but not populated on Rev.C and Rev.D:

waclawekjan_0-1712657455335.png

If it is populated on Rev.E, UM1472 fails to mention that in the revisions changelog:

waclawekjan_1-1712657551638.png

And in any case, absence of R31 in Revs. C and D should be mentioned in conjunction with SB18 in Table 6. Solder bridges.

JW

 

PS. Please restore the schematics (of the last rev.) in the UM, for convenience of the users. Please add links to schematics for the older revs. into the UM. When updating the UM, please don't use the bad "modern feel and look" color scheme.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
STTwo-32
ST Employee

Hello @waclawek.jan 

I've escalated your request to the Concerned to team for update (Under internal ticket number 178598)

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.