2024-08-01 05:29 PM
Hello,
We encountered that Necleo-F756 could not auto-start program with the E5V(+5V), VDD(+12V) external power input.
but it can auto start with USB (ST-Link) power input. I think there is something wrong with the settings. Our setting is below. Could you give me any advice?
[Settings]
1. Power input : +5V => CN11 pin 6 (E5V) , J3 jumper connect between 2 and 1 (E5V) , JP1 no jumper.
2. STM32CubeProbgrammer : check Run after Programing
I attached the Excel file for the details of the Nucleo setting, NRST wave and STM32CubeProgrammer setting.
2024-08-02 03:46 PM
Hello @Kusagaya
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Roger