2024-08-30 03:43 AM
Hello,
I am trying to use RF with iOS and Android to write into the memory of the ST25DV04KC. Reading is not a problem, but the difficulty is the protection. There are two areas: Area 1 is only used for the NDEF message and is locked with Password 1. Area 2 is the data area, which is also protected with Password 1. So, reading does not require a password, but writing with RF into the area does.
I studied the datasheet, and it looks very confusing. I can't figure out how to handle writing multiple blocks into an area that is password-protected.
Here is more information: I initially used the Req_Flag, which is 0x62 or 0x22, with the ID of the chip. The command for multiple block writes is 0x24, and the starting block is 0x0A (which is Block 11). To write two blocks, I use 0x01 (because the number of blocks is -1). I also saw that the maximum number of blocks is 4, so the maximum number of blocks to write in the data area is 0x03. When I issue these commands with the NFC Tag app, it says that the area is password-protected.
So, I understand that the area is protected by a password, which is Password 1 (0x01). The current password is actually 0, but I should change it later. The password format is (0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00).
Could someone explain an example of the commands to write over RF into the memory with this data I provided?