2021-01-25 01:37 AM
Hi,
I use a X-NUCLEO-NFC06A1shield and a Nucleo-476RG to read a NFC chips ( M24LR64D-W or M24LR04).
For my test I use the demo program from ST provided with the shield.
I want to read 32 blocks (a block is 4 bytes) with the function rfalNfcvPollerReadMultipleBlocks.
If the numOfBlocks parameter is set to 31 the function works correctly.
If the numOfBlocks parameter is set to 32 the function returns ERR_REQUEST.
Could you help me to resolve this issue?
Thx & Regards
Nigoros
Note 1: The chip M24LR04 is on a red board M24LR-discovery.
Note 2: To read the chip M24LR64D-W I use the function rfalST25xVPollerM24LRReadMultipleBlocks with the same issue.
Solved! Go to Solution.
2021-01-25 05:00 AM
Hi,
the M24LR04 supports a maximum of 32 blocks in one Read Multiple Blocks command (see M24LR04E-R Datasheet §26.5 "The maximum number of blocks is fixed at 32 assuming that they are all located in the same sector"). The number block is encoded in numOfBlocks minus 1 i.e. a value of '06' in the "Number of blocks" field requests to read 7 blocks. A value of '00' requests to read a single block.
When setting numOfBlocks to 32, this actually requests 33 blocks and the tag returns an error.
Using numOfBlocks = 31 will return 32 blocks
Rgds
BT
2021-01-25 05:00 AM
Hi,
the M24LR04 supports a maximum of 32 blocks in one Read Multiple Blocks command (see M24LR04E-R Datasheet §26.5 "The maximum number of blocks is fixed at 32 assuming that they are all located in the same sector"). The number block is encoded in numOfBlocks minus 1 i.e. a value of '06' in the "Number of blocks" field requests to read 7 blocks. A value of '00' requests to read a single block.
When setting numOfBlocks to 32, this actually requests 33 blocks and the tag returns an error.
Using numOfBlocks = 31 will return 32 blocks
Rgds
BT
2021-01-25 06:25 AM
Super!
I take into account your response and now it works.
The header of the function is not very verbose about it.
Thx & regards
2021-01-25 07:09 AM
Hi,
Actually, numOfBlock is the number of blocks to read in addition to the one specified by firstBlockNum. This numOfBlocks parameter follows ISO/IE 15693-3 encoding of "number of blocks" in read Multiple Blocks command.
I will anyhow report your feedback to the developers.
Rgds
BT