cancel
Showing results for 
Search instead for 
Did you mean: 

which rf command cr95hf need to send on message receive from tag ?

Mpraj.19
Associate II

my setup is st25dv04k connected with tag on instrument A. cr95hf connected with instrument B. when instrument A comes near to instrument B.

i want to confirm that instrument be successfully message in a tag [ which connected to instrument A].

on successful reading data by cr95hf , is it possible to send rf command over air to st25dv04k ? also which rf command it need to send ?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Brian TIDAL
ST Employee

Hi Mpraj.19

the CR95HF is a RF transceiver therefore you can send whatever you want to the tag using the SendRecv command.

The ST25 Embedded NFC library provides examples of communication between ST25 Readers and ST25DV tags (e.g. see Projects\STM32L476RG-Nucleo\Applications\X-NUCLEO-NFC03A1\FTM example).

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Brian TIDAL
ST Employee

Hi Mpraj.19

the CR95HF is a RF transceiver therefore you can send whatever you want to the tag using the SendRecv command.

The ST25 Embedded NFC library provides examples of communication between ST25 Readers and ST25DV tags (e.g. see Projects\STM32L476RG-Nucleo\Applications\X-NUCLEO-NFC03A1\FTM example).

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Mpraj.19
Associate II

The given software in exe format can you provide same software or source file for linux.

Brian TIDAL
ST Employee

Hi,

the exe contains a click through license that needs to be accepted so this exe has to be downloaded on a Windows PC, the license has to be accepted and then you can copy the files on your Linux environment.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.