2017-11-27 10:05 PM
What is the device address of the M24LR64 - R? I am studying I2C using X-NUCLEO-NFC 02 A 1. X-NUCLEO-NFC02A1 has EEPROM (M24LR64-R). However, I do not know the device address of the M24LR64 - R. Even if I looked at the data sheet, I could not understand where it is written because of beginners. I am happy if you give me a hint.
Best Regards,
Ken Inoue
Solved! Go to Solution.
2017-11-28 12:10 AM
Does the X-NUCLEO-NFC02A1 user manual say something about it ?
Checking the M24LR64-R datasheet,it says:
The device select code consists of a 4-bit device type identifier, and a 3-bit Chip Enable “Address� (E2, E1, E0). To address the memory array, the 4-bit device type identifier is 1010b.
Address bits E1 and E0 are defined by external pins, so check the schematics.
E2 depends on the memory range you want to access.
2017-11-28 12:10 AM
Does the X-NUCLEO-NFC02A1 user manual say something about it ?
Checking the M24LR64-R datasheet,it says:
The device select code consists of a 4-bit device type identifier, and a 3-bit Chip Enable “Address� (E2, E1, E0). To address the memory array, the 4-bit device type identifier is 1010b.
Address bits E1 and E0 are defined by external pins, so check the schematics.
E2 depends on the memory range you want to access.
2017-11-30 1:21 AM
Dear Mr./Ms. AvaTar
Thanks to you I understood.
Thanks.
Best Regards,
Ken Inoue