cancel
Showing results for 
Search instead for 
Did you mean: 

What are the 27.12MHz crystal specification for the ST25R3916? The evaluation kit uses Murata XRCGB27M120F3M00R0, which is 30ppm tolerance, 40ppm stability, 6pF load capacitance. Can we use a 100ppm tolerance version, XRCGB27M120F0Z00R0?

Ade G.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Travis Palmer
ST Employee

Hello,

the crystal tolerance is mainly given by the standard you want to comply with.

For ISO14443 it is stated: "The frequency fc of the RF operating field shall be 13,56 MHz ±7 kHz.".

Which means your crystal frequency drift should not be more then +/-7kHz in total.

BR Travis

View solution in original post

1 REPLY 1
Travis Palmer
ST Employee

Hello,

the crystal tolerance is mainly given by the standard you want to comply with.

For ISO14443 it is stated: "The frequency fc of the RF operating field shall be 13,56 MHz ±7 kHz.".

Which means your crystal frequency drift should not be more then +/-7kHz in total.

BR Travis