cancel
Showing results for 
Search instead for 
Did you mean: 

I just needed to understand the read ranges achieved with the help of ST25R3911B-DISCO VS X-NUCLEO-NFC05A and ST25R3916-DISCO VS X-NUCLEO-NFC06A, the application I'm working on required the read ranges anywhere about 10cm

RMaha.1
Associate
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Travis Palmer
ST Employee

Hello,

The read range which can be achieved will mainly be defined by the used antenna size. The bigger the antenna the bigger the read range will be if there is sufficient coupling between reader and tag antenna. In other words if you increase your reader antenna and have a very small tag antenna, the read range might even reduce.

Also the used technology will influence the achievable read range. ISO15693 for example will have a bigger read range then ISO14443.

Looking only at the antenna sizes, the two DISCO boards will give you the biggest read range. The two X-NUCLEO-NFC05/06 boards will have approximately the same read range.

There are several interesting posts which discuss how to increase the read range:

https://community.st.com/s/question/0D50X00009XkWCSSA3/design-questions-around-st25r3911b

https://community.st.com/s/question/0D50X0000Bh5zQqSQI/how-to-use-st25r3911b-for-long-reading-distance40cm

In general I would state the read range of the DISCO's 1-2 times higher then the X-NUCLEO-NFC05/06 depended on the used technology and card (antenna size and resonance frequency).

Please let me know, if this answers your question.

BR Travis

View solution in original post

1 REPLY 1
Travis Palmer
ST Employee

Hello,

The read range which can be achieved will mainly be defined by the used antenna size. The bigger the antenna the bigger the read range will be if there is sufficient coupling between reader and tag antenna. In other words if you increase your reader antenna and have a very small tag antenna, the read range might even reduce.

Also the used technology will influence the achievable read range. ISO15693 for example will have a bigger read range then ISO14443.

Looking only at the antenna sizes, the two DISCO boards will give you the biggest read range. The two X-NUCLEO-NFC05/06 boards will have approximately the same read range.

There are several interesting posts which discuss how to increase the read range:

https://community.st.com/s/question/0D50X00009XkWCSSA3/design-questions-around-st25r3911b

https://community.st.com/s/question/0D50X0000Bh5zQqSQI/how-to-use-st25r3911b-for-long-reading-distance40cm

In general I would state the read range of the DISCO's 1-2 times higher then the X-NUCLEO-NFC05/06 depended on the used technology and card (antenna size and resonance frequency).

Please let me know, if this answers your question.

BR Travis