2022-08-08 03:03 PM
Hello,
I would like to receive information on the thermal characteristics of ST25R3916-AQWT.
Rja and Rca.
Let me know your input!
Cheers
Madhu
Solved! Go to Solution.
2022-08-11 06:36 AM
Hello Madhu,
Rtheta_jc is specific to the device (more in detail it is specific to the used package).
This is why we can very precisely can name this number.
Rthetha_ja is specific to the device / package, PCB (size, amount of copper, number of layers, ...) and housing / airflow. This means, this number (Rthetha_ja) is specific to the application itself and we cannot do a general statement here.
This is why we did this application note, showing how to setup the thermal model and measure / calculate the thermal resistance of each node (e.g. ja an ca on bottom and top).
BR Travis
2022-08-09 02:46 AM
2022-08-09 10:24 AM
Hello Ulysses,
I did check the document. I was able to find Rtheta_jc as 16.95C. I dont think Rthetha_ja is not listed if I am right. So is it possible to get the correct value for Rthetha_ja?
Cheers
Madhu
2022-08-11 06:36 AM
Hello Madhu,
Rtheta_jc is specific to the device (more in detail it is specific to the used package).
This is why we can very precisely can name this number.
Rthetha_ja is specific to the device / package, PCB (size, amount of copper, number of layers, ...) and housing / airflow. This means, this number (Rthetha_ja) is specific to the application itself and we cannot do a general statement here.
This is why we did this application note, showing how to setup the thermal model and measure / calculate the thermal resistance of each node (e.g. ja an ca on bottom and top).
BR Travis