2024-02-06 3:47 PM
Hi,
I am new to NFC therefore using the kit as a starting point. I learnt that we can use the following tools to design the antenna:-
Question 1
If I am using the tool (https://eds.st.com/antenna/#/) to help design the antenna and to find the right capacitance for the matching network,
what sort of data(the field marked with ?) should I enter on the page as shown below?
Geometry
Turns: 2
Antenna Length: ? mm
Antenna Width: ? mm
Conductor
Width: ? mm
Spacing: ? mm
Thickness: ? um
Substrate
Thickness: ? mm
RElative Electrical Permittivity: ?
Resonant freq: 13.56MHz
Question 2:
Can you provide me with the value of the antenna inductance?
Thanks in advance!!!
Best Regards,
Cindy
Solved! Go to Solution.
2024-02-07 12:25 AM
2024-02-07 12:25 AM
Hi Cindy,
please study AN5276 and AN5322.
BR, Ulysses