cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-25R20SA Eval kit won't respond

hfarooqui
Associate II

Hi, 

Every time I try to connect the eval kit to the GUI I get this error:

This board doesn't reply properly to connect !

Can anyone tell me how to solve this problem.  I have made sure that the correct COM Port and baud rate is selected. Also, the power indicator LED is ON and the RED LED is flashing. 

Your help is greatly appreciated.

Regards,

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hi,

yes, check the points from Brian. IMO most probable: USB cable: Check it has a USB symbol and not a battery symbol. Verify with a different device that it works.

Ulysses

View solution in original post

11 REPLIES 11
Brian TIDAL
ST Employee

Hi,

make sure the baud rate is 921600.  Make sure there no other STLink device connected. Try to flash the firmware (click on the Update firmware button on the main tab) in case the flash has been erased or modified. If it is still not working, could you send the content of the logging window?

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

The content of the logging window is as follows:

0: serEncSysNfcResetReq()

1: serEncSysNfcResetReq()

2: serEncSysNfcResetReq()

3: serEncSysNfcResetReq()

It will not let me update firmware as it doesn't properly connect to the board.

 

The baud rate is sent to 921600 for both COM port and the board

Hi,

the update firmware button is available even when the connect has failed. The firmware update uses the mass storage feature of the STLink. When clicking on the update firmware, you can select the proper device (25R200A) and start the firmware download. 

In case the mass storage is blocked by your organisation, you can use STM32CubeProgrammer to download the firmware (you can retrieve the firmware location from the STEVAL-25R200 GUI update firmware window). 

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
hfarooqui
Associate II

How do I use the STM32CubeProgrammer?

The firmware directory that the GUI is pointing to has nothing in it.

This is what the firmware update screen looks like.

 

Hi,

when clicking on Scan board in the upgrade firmware window, nothing is displayed? Copy the "FW dir": this contains the binary.

For STM32CubeProgrammer, go on st.com and download the installer. Start STM32CubeProgrammer, click on connect. If you cannot connect, check your USB cable. Open the "FW dir" and load the FW onto the board.

Rgds

BT

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Yes, nothing comes up when I press Scan boards.

I will try the STM32Cubeprogrammer and try to connect via the programmer.

The STM32Cubeprogrammer isn't connecting either.