cancel
Showing results for 
Search instead for 
Did you mean: 

ST25RU3993-HPEV read tags in 3ft only

YChav.3
Associate II

At ST25RU3993-HPEV firmware how to control an antenna distance? For eg. I want an antenna to read tags in 3ft only.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Nick K
ST Employee

Hello YChav.3

In general the read range can be limited with the TX power settings. The less Tx power the less read range. A strong dependency is also given through the used antenna. Also the used Tag and frequency can have a impact on the read range. This means one Tx power settings can limit the read range for one setup, but could allow to read further with a different setup.

BR

Nick

View solution in original post

1 REPLY 1
Nick K
ST Employee

Hello YChav.3

In general the read range can be limited with the TX power settings. The less Tx power the less read range. A strong dependency is also given through the used antenna. Also the used Tag and frequency can have a impact on the read range. This means one Tx power settings can limit the read range for one setup, but could allow to read further with a different setup.

BR

Nick