2024-08-28 03:18 AM
Hi,
I’m working with an ST25R3916B custom board connected via SPI to a custom embedded Linux system. The system is running the ST25R3916_v2.8.0_Linux_demo_v1.0, but it is unable to detect any NFC tags.
The issue seems to originate from the nfc_demo_st3916b application, specifically in st25r3916.c at the st25r3916OscOn() function. The application fails at the check on ST25R3916_REG_AUX_DISPLAY_osc_ok at line 287. To bypass this, I commented out the check, which allowed the application to run, but it still does not detect any tags.
Here’s what I’ve observed:
I would greatly appreciate any advice or recommendations on what further steps I should take to resolve this issue.
Thank you and best regards,
Dave