2022-09-21 5:02 AM
Which ST25R reader would you recommend for the MB89R118C Fujitsu Tag which has FRAM of 256 memory blocks/ 2048 bytes and uses ISO/IEC15693? For some reasons I could not write or read from this NFC type 5 tag with the NFC Tap app? Please advise.
Solved! Go to Solution.
2022-09-21 5:11 AM
Hi,
MB89R118C is a 8-byte per block device. This can be read by any of the ST25R device (ST25R95, ST25R3911B or ST25R3916/3916B).
In ISO/IEC15693 mode, NFC Tap app is limited to 4-byte per block device thus MB89R118C cannot be read by this app.
Rgds
BT
2022-09-21 5:11 AM
Hi,
MB89R118C is a 8-byte per block device. This can be read by any of the ST25R device (ST25R95, ST25R3911B or ST25R3916/3916B).
In ISO/IEC15693 mode, NFC Tap app is limited to 4-byte per block device thus MB89R118C cannot be read by this app.
Rgds
BT
2022-09-21 5:16 AM
Thank you so much! Would you recommend another app that may do 8-byte per block if any?
2022-09-21 5:27 AM
Well, difficult for me to recommend an app from the competition ;) but if you google "app NFC Tag Info", you should find some apps.
Rgds
BT