cancel
Showing results for 
Search instead for 
Did you mean: 

M24LR-E energy harvesting

So.Sunny
Associate II
Posted on March 23, 2016 at 11:57

I test with 24LR04e-discovery board..Use CR95HF demo board to set EH enable-03,and 

EH Config-F3. Put board near wire and the board can display message. But if I set F0 and mean max 7mA. It is very difficult to drive the board message display. I measure the VDD output and always about 0.5V. Why set max current higher not better ? How can i set to output more current to 7mA?  thanks

#m24lr04e
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Nickname5101_O
Associate II
Posted on October 18, 2016 at 08:46

Increase the range doesn't change the power capability of M24LR it only change the current trigger value to start delivery , this mean if your applictaion need  3mA set the caliber to 3mA  EH will be set only if 3mA are available , if not  EH will remain Hz .

(Probably what happen in your case when you choose 7mA caliber)

View solution in original post

1 REPLY 1
Nickname5101_O
Associate II
Posted on October 18, 2016 at 08:46

Increase the range doesn't change the power capability of M24LR it only change the current trigger value to start delivery , this mean if your applictaion need  3mA set the caliber to 3mA  EH will be set only if 3mA are available , if not  EH will remain Hz .

(Probably what happen in your case when you choose 7mA caliber)