Skip to main content
JPark.21
Associate
December 27, 2020
Solved

Is X-Nucleo-NFC03A1 board compatible with Arduino Uno?

  • December 27, 2020
  • 3 replies
  • 1412 views

I have purchased "X-Nucleo-NFC03A1" NFC reader evaluation board. Can I use Arduino Uno to control the NFC board? and does anyone have a sample library?

    This topic has been closed for replies.
    Best answer by parata.carlo

    Hi,

    the X-NUCLEO-NFC03A1 library is currently compatible only with stm32duino boards. The job to make it compatible also with Arduino Uno should not so difficult because basically the board uses the standard APIs of Arduino framework. I suppose that there are some typedef and define to adjust in order to remove some errors that you can get with Arduino UNO target. Anyway, I'm not sure that Arduino UNO has enough flash and RAM memories to run the X-NUCLEO-NFC03A1 library.

    Best Regards,

    Carlo

    3 replies

    Brian TIDAL
    ST Technical Moderator
    January 4, 2021

    Hi,

    you can find a sample lib here https://github.com/stm32duino/X-NUCLEO-NFC03A1

    there is also another library  for Arduino. This is originally for the BM019 board but should run with X-NUCLEO-NFC03A1 with no or only little changes.

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    JPark.21
    JPark.21Author
    Associate
    January 4, 2021

    Thank you for your help, Brian.

    I am using Arduino Uno R3 to control X-Nucleo-NFC03A1. I got the following error message while uploading the sample code in the library.

    "WARNING: library X-NUCLEO-NFC03A1 claims to run on stm32 architecture(s) and may be incompatible with your current board which runs on avr architecture(s)"

    I am wondering that I can use Arduino Uno for X-Nucleo-NFC03A1. or, should I use stm32duino board?

    Regards,

    JYP

    parata.carlo
    parata.carloBest answer
    ST Employee
    January 5, 2021

    Hi,

    the X-NUCLEO-NFC03A1 library is currently compatible only with stm32duino boards. The job to make it compatible also with Arduino Uno should not so difficult because basically the board uses the standard APIs of Arduino framework. I suppose that there are some typedef and define to adjust in order to remove some errors that you can get with Arduino UNO target. Anyway, I'm not sure that Arduino UNO has enough flash and RAM memories to run the X-NUCLEO-NFC03A1 library.

    Best Regards,

    Carlo