cancel
Showing results for 
Search instead for 
Did you mean: 

Increase reading distance of CR95HF

chris1911
Associate II

Currently, I'm using CR95HF on our product which went into mass production already.  The tag is small with diameter only 9mm.  In the field, we are seeing a few percentage of unsuccessful read from the first read and need to retry several times.  How can we increase reading distance?  Is it possible to boost the transmit power from the reader chip?

The tag has NTAG213 on it.  Our reader antenna is in octagon shape.

 

chris1911_0-1710998627148.png

 

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Of course, it would be ideal if both the tag and reader antenna were significantly larger.

But even if the tag remains the same size, you will achieve slightly better results with a larger reader antenna. You can also test this without a new PCB by cutting off one of the PCB coils and connecting a wire coil with different diameters to the vias.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
chris1911
Associate II

Right now, we are using 3.3V for both VPS_Main and VPS_TX.  I'm think if we keep 3.3V for VPS_Main and use 5V for VPS_TX, we should get a higher RF power.  A higher RF power probably will increase the reading distance.  Do you think this will work?

Peter BENSCH
ST Employee

Welcome @chris1911, to the community!

You won't experience a significant change in range with this slightly higher voltage. You have a significantly greater influence on this with larger antenna geometries, both at the reader and the tag. Since the tag is apparently fixed, you can only try to achieve more range with a larger reader antenna.

What dimensions does the reader antenna currently have?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
chris1911
Associate II

Hi Peter,

Thanks for your comment.  Below picture show our reader antenna size which is slightly larger than the Tag which is 9mm in diameter.  We have three readers in a row to check three tags but only one reader is enable at the same time.  The distance between the antenna and the tag is about 8mm.  Will we get better reading distance with a bigger antenna?  What size will you suggest us to try?

 

Regards,

Chris

chris1911_0-1711092616924.png

chris1911_1-1711092659388.png

 

Peter BENSCH
ST Employee

Of course, it would be ideal if both the tag and reader antenna were significantly larger.

But even if the tag remains the same size, you will achieve slightly better results with a larger reader antenna. You can also test this without a new PCB by cutting off one of the PCB coils and connecting a wire coil with different diameters to the vias.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.