2023-05-05 2:12 PM
I have program for CAN bus and NFC08a1 but when i combine i get several errors. All i want to do is get the reading from the nfc reader and send them on can. does anyone know how to do that?
Solved! Go to Solution.
2023-05-15 10:54 AM
Hi,
make sure to keep platformErrorHandle aligned with the error handler function defined in the main.c (i.e. Error_Handler).
The SPI settings are incorrect vs the ST26R3916B Datasheet .:
Rgds
BT
2023-05-15 10:59 AM
ok i get it.
2023-05-15 11:10 AM
the field led field is very dim and when i put a nfcv the ledv doesn't turn on. it only blinkes like led field
2023-05-15 11:13 AM
hi,
can you now provide the logic analyzer trace?
rgds
BT
2023-05-15 12:05 PM
2023-05-15 12:45 PM
Hi,
can you add the IRQ_3916B signal and send to me the salae file so that I can analyze it (I can do nothing with a screen shot).
Thanks
Rgds
BT
2023-05-15 12:48 PM
it wont let me send sal file here.
2023-05-15 1:05 PM
zip it and send it to me in private message
2023-05-15 1:09 PM
2023-05-15 1:14 PM