cancel
Showing results for 
Search instead for 
Did you mean: 

I find the X-Nucleo-NFC06A1 antenna has higher inductance than the 3916-DISCO. Could somebody explain please?

SSita
Associate

The X-NUcleo-NFC06A1 measure ~1.3uH, whereas the ST25R3916-DISCO measures close to 1uH.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Travis Palmer
ST Employee

Hello SSita,

The dimension of the Antenna (width, length and number of turns) mainly define its inductance value. Other parameters are trace width and distance between the antenna turns.

You can use the antenna design tool of ST's eDesign suite to estimate the antenna inductance.

BR Travis

View solution in original post

1 REPLY 1
Travis Palmer
ST Employee

Hello SSita,

The dimension of the Antenna (width, length and number of turns) mainly define its inductance value. Other parameters are trace width and distance between the antenna turns.

You can use the antenna design tool of ST's eDesign suite to estimate the antenna inductance.

BR Travis