Skip to main content
Associate II
February 9, 2026
Question

Sensorless FOC Observer Reports High Speed during Startup

  • February 9, 2026
  • 2 replies
  • 254 views

[PN]: NUCLEO-G431RB with EVLDRIVE102BH and custom motor

[VERSION]: Version: 6.4.1 Build: 250722.104358
[TOOL]: Motor Control Pilot
[DETAILS]:

Hello All,

I have been working on getting a sensorless FOC driver to work. So far I am able to get the rotor to align and move under open-loop control and occasionally it can switch over to closed loop control. When the motor switches over and runs it is fairly stable. My main issue is that I am unable to get the motor to reliably make the switch from open loop to closed loop. When it fails I often get a speed error with FAULT_OVER. I am using the STO+PLL Observer and I have gone through the current loop tuning and I think that looks good, the speed loop could use a little more work once this is resolved, but if the issue is with the observer I don't want to spend too much time on it yet.

I output the BEMF-A and BEMF-B signals through the DAC to an oscilloscope, and when the startup fails I see both the amplitude and the frequency of the BEMF signals become far larger than I would ever expect to see in application (motor pilot reports 50krpm+) which makes me think that the FAULT_OVER error is real and that the BEMF signal calculations are either getting bad data in or that the observer loop needs more work. I am using a low inductance motor and I can see the FETs switching on the BEMF waveforms also adding to the noise.

How should I go about diagnosing and resolving this issue?

 

2 replies

GMA
ST Technical Moderator
February 10, 2026

Hello @pdiefend_GLO,

Do you mean "Speed feedback error"?

For error description and management, refer to the documentation available through the Workbench tool: About > Documentations > Documentation > User manual tab, (FOC) firmware errors link.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
Associate II
February 10, 2026

yes, speed feedback error. The error is real, I can see it happening on the oscilloscope. I'm trying to determine the root cause.