2026-05-12 7:32 PM
I am designing a LED driver board for an industrial instrument and am evaluating the ST1CC40 as a constant-current buck driver for the following application:
Application requirements:
• Input voltage: 5V DC (regulated)
• LED: Cree XLamp XP-L2 white LED
• Target forward current: 2.2A
• LED forward voltage: 3V at 2.2A, Tj = 85°C
From the ST1CC40 datasheet, I have confirmed the following:
• VIN range 3V–18V covers our 5V supply
• Maximum limiting current 5A covers our 2.2A operating point
• INH threshold VIH = 1.2V min is compatible with our 3.3V PWM signal
• Duty cycle at operating point: 2.93V / 5V = 58.6% — within range
• RSENSE = 97mV / 2.2A = 44mΩ (targeting 44mΩ E96 standard value)
I have the following technical questions:
1. With VIN = 5V and VOUT ≈ 2.93V (duty cycle ~58.6%), is there any concern with the internal bootstrap circuit or headroom voltage at this relatively low input voltage/ application?
2. For inductor selection at VIN = 5V, VOUT = 2.93V, ILED = 2.2A, FSW = 850kHz, could you confirm the recommended inductance value and saturation current rating? I intend to use the eDesignSuite tool but would welcome any guidance.
I am designing for an industrial instrument and reliability is a primary concern. Any guidance on derating or thermal recommendations for the SO-8 package at 2.2A continuous would also be appreciated.
2026-05-12 11:56 PM
Welcome @iyer_22, to the community!
For the SO-8 thermal design at 2.2A continuous, good PCB copper area, thermal vias, and a conservative derating approach are strongly recommended. Also, the sense resistor dissipation is non-negligible and should be included in the thermal budget. Please use the EVAL boards STEVAL-ILL046V1 and STEVAL-ILL046V2 as a template and, depending on the maximum ambient temperature, feel free to equip them with larger cooling surfaces.
Hope that helps?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.