cancel
Showing results for 
Search instead for 
Did you mean: 

How do I use the NFC07A1_NFCTAG_WriteData function?

Schuyler
Senior

I need to write a specific string to the ST25 tag, but I don't see the use of NFC07A1_NFCTAG_WriteData. What should I do so that the string is written to the tag's address correctly and can be read by NFC?

/**
  * @brief  Writes data in the nfctag at specific address
  * @PAram  pData : pointer to the data to write
  * @PAram  TarAddr : I2C data memory address to write
  * @PAram  Size : Size in bytes of the value to be written
  * @retval NFCTAG enum status
  */
int32_t NFC07A1_NFCTAG_WriteData( uint32_t Instance, const uint8_t * const pData, const uint16_t TarAddr, const uint16_t Size )
{
  UNUSED(Instance);
  if ( Nfctag_Drv->WriteData == NULL )
  {
    return NFCTAG_ERROR;
  }
  
  return Nfctag_Drv->WriteData(&NfcTagObj, pData, TarAddr, Size );
}
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0