cancel
Showing results for 
Search instead for 
Did you mean: 

How do I enable the Fast Transfer Mode (FTM) for writing into the Mailbox of the X-NUCLEO-NFC07A1 ?

Schuyler
Senior

0693W00000aJ0zfQAC.png我正在使用X-NUCLEO-NFC7A07的软件“x-cube-nfc1�?。�?幸的是,我无法�?�用FTM模�?。我有点困惑,因为NDEF无法接收信�?�,但是我找�?到项目中的具体代�?。

Translation to english:

I am using the software "x-cube-nfc1" of X-NUCLEO-NFC7A07. Unfortunately, I cannot enable FTM mode. I'm a bit confused because NDEF can't receive the information, but I can't find the specific code in the project.

1 ACCEPTED SOLUTION

Accepted Solutions
Brian TIDAL
ST Employee

Hi,

X-CUBE-NFC1 is designed to work with X-NUCLEO-NFC01A1 expansion board.

For X-NUCLEO-NFC07A1 board, make sure to use X-CUBE-NFC7 package.

Rgds

BT

P.-S.: this community uses English language.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Brian TIDAL
ST Employee

Hi,

X-CUBE-NFC1 is designed to work with X-NUCLEO-NFC01A1 expansion board.

For X-NUCLEO-NFC07A1 board, make sure to use X-CUBE-NFC7 package.

Rgds

BT

P.-S.: this community uses English language.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.