2020-07-07 01:59 AM
Hi,
I am assessing to use CR95HF, ST95HF or ST25R95 for a low power access control reader application and I have a question.
I would like to know if thre is any difference between thse 2 parts:
Regards, Ramon.
Solved! Go to Solution.
2023-06-01 05:48 AM
Hi Brian TIDAL,
Would you please elaborate how to port CR95HF library to other than ST MCU
2023-06-02 12:24 AM
Hi,
I would recommand not to post on an old and already answered thread (to avoid never ending thread) Feel free to enter a new thread.
Rgds
BT.
2023-10-23 03:27 AM
Hi, still wondering about the differences between ST95HF and ST25R95. I understand from this Q&A's they are identical, but in specification "Reset the ST95HR - MOSI 00000001" and "Reset the ST2595 - MOSI 00000000". In considering to change old ST95 to newer ST25R95 but is there something else exist I need to change in SW?
2023-10-23 04:31 AM
Hi,
I would suggest to create a new thread rather that posting on an already answered thread. As far as I know the reset control byte is identical on CR95HF, ST95HF and ST25R95: 0x01 (see §4.1.1 in the ST25R95 datasheet). And no FW change is needed when moving from ST95HF to ST25R95. Feel free to create a new thread if you need more information.
Rgds
BT