2021-03-12 06:44 AM
Is it possible to use ST25R3916 capacitive wake-up outdoors? The reading area can be wet, frozen or snow covered.
Solved! Go to Solution.
2021-03-12 07:38 AM
Hello Stinde,
When the reader is mounted outdoor using a propper housing there should be no problem for that.
For both, capacitive and inductive wake-up apply the same rule:
If the environment changes ( = temperature, metal in close proximity, moisture (mainly influencing capacitive wake-up),..) then the reader will wake-up.
You can then either use automatic averaging which helps filtering those effects or just re-arm the wake-up if no tag has been found.
br Travis
2021-03-12 07:38 AM
Hello Stinde,
When the reader is mounted outdoor using a propper housing there should be no problem for that.
For both, capacitive and inductive wake-up apply the same rule:
If the environment changes ( = temperature, metal in close proximity, moisture (mainly influencing capacitive wake-up),..) then the reader will wake-up.
You can then either use automatic averaging which helps filtering those effects or just re-arm the wake-up if no tag has been found.
br Travis
2021-03-13 01:34 AM
Hi Travis,
I was thinking since capacitive wake-up is sensing water in human hand. If there is a layer of water between the sensor and hand, can the capacitive sensor really detect the hand behind the water layer. I know the averaging can help in slowly changing environment, but is the water layer close to sensor plates acting as a short circuit for electric field?
Best Regards,
Stinde