cancel
Showing results for 
Search instead for 
Did you mean: 

c# visual studio ST25R3916_Interface.cs ST25R391x_Dll.iso15693TxRxNBytes

GDC
Associate II

I'm in trouble using dll with c# for using the mailbox.

Can someone help me?

Please @Ulysses HERNIOSUS , my friend, help me! I'm pain too!

 

Here is the code:

 

private void TxRxNBytes_Click(object sender, EventArgs e) {//This is a button click event handler

    sbyte[] rx = new sbyte[512];

    //Here following is the reversed uid byte sequence compared to the one reported from software ST25PC-NFC
    byte[] uid = [0x61, 0x92, 0x74, 0xD0, 0x01, 0x24, 0x02, 0xE0];

    

    ee = ST25R391x_Dll.iso15693Select(Handle, uid);    // ee=NoError

    sbyte[] tx = { 0x10 , unchecked((sbyte)0xAA) , 0x02 , 0x06 , 0x01 , 0x02 , 0x03 , 0x04 , 0x05 , 0x06 };

    ee = ST25R391x_Dll.iso15693TxRxNBytes(Handle, tx, 10, rx, ref uRxDim, 1);    //    ee=NoError...

 

// ... but microcontroller hosting ST25DV04K doesn't receve the GPO signaling.
//   Instead, using software ST25PC-NFC -> Fast Transfer Mode -> WriteMessage , the microcontroller hosting

//    ST25DV04K hit an interrupt due to MB_CTRL_Dyn -> RF_PUT_MSG and reading the mail box results the  

//    exact sequence {0x01,0x02,0x03,0x04,0x05,0x06}

 

What i'm doing wrong?
Can someone help me?

 

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Brian TIDAL
ST Employee

Hi,

what are the values of the GPO and GPO_CTRL_Dyn registers? is the Write Message (0xAA) command successful, if not, what is the return code? Be aware that "MSGlength" parameter of the command is the number of Data bytes minus 1 (see §7.6.31 Write Message in the Datasheet). So, the MSGLength should be 05 for "01 02 03 04 05 06"

Rgds

BT

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Brian TIDAL
ST Employee

Hi,

what are the values of the GPO and GPO_CTRL_Dyn registers? is the Write Message (0xAA) command successful, if not, what is the return code? Be aware that "MSGlength" parameter of the command is the number of Data bytes minus 1 (see §7.6.31 Write Message in the Datasheet). So, the MSGLength should be 05 for "01 02 03 04 05 06"

Rgds

BT

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.