cancel
Showing results for 
Search instead for 
Did you mean: 

What is the difference between the obsolete VNS1NV04D-E and the new VNS1NV04DP-E? Thanks, Jim

JMall.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @JMall.1​, to the community!

The dies inside are identical, but the internal connection is a bit different. This means that apart from the maximum total power dissipation, the electrical parameters are completely identical.

The thermal resistance Rthj-lead increased from 15K/W (VNS1NV04D-E) to 30K/W (VNS1NV04DP-E), so the absolute maximum total power dissipation decreased from 8.3W to 4W, which must be taken into account for the cooling measures.

Good luck!

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.