2021-07-06 5:33 AM
Hi all,I need some help to know what is the reference of this component ? I can read ST e3 G FBo Z205 but it's impossible to find something like that on the net to purchase it. I need 2 of its. I'm in France if you have a resealer which is seeling this?
Is it a kind of Zener diode ? if yes what ios the correct ref to purchase it?
Best Regards
2021-07-06 5:39 AM
maybe reference is ST e3 G also ?
2021-07-06 6:41 AM
e3 refers to the metal or tinning as I recall
FBO SMCJ24CA-TR https://www.st.com/en/protection-devices/smcj24ca.html
Bidirectional TVS diode
2021-07-06 6:44 AM
Couple of people make equivalents
https://octopart.com/search?q=SMCJ24CA¤cy=USD&specs=0
2021-07-06 7:04 AM
thank you, how do you know that this is this ref SMCJ24CA ?
2021-07-06 7:16 AM
2021-07-06 8:59 AM
Cause that's what the datasheet says it is, along with the information that it's the Bidirectional TVS, which can also be observed from the lack of a white bar conferring direction
https://www.st.com/resource/en/datasheet/smcj24ca.pdf
2021-07-06 9:02 AM
Might want to look at what actually failed there, diodes seem to have conducted more than the traces
2021-07-06 9:06 AM
I hope no but I will change the diode and see if the relay behind is ok or not.
This is a card for a swimming pool roller shutter and in manual position I can open and close the shutter, I cross the fingers :anxious_face_with_sweat:
thanks for the big help :ok_hand: