cancel
Showing results for 
Search instead for 
Did you mean: 

We use the VNH3SP30 H-bridge motor driver for an application where we need to drive a motor with peak currents over 30A. The PCB layout are made following the recommendations from datasheet. But the H- bridge die when running the motor. Any help?

NCalm.1
Associate

Is external protection needed?

And what type off protection if it also should be able to handle EMC Burst and Surge pulses?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0