2018-05-12 10:44 AM - last edited on 2023-08-31 12:19 AM by Peter BENSCH
Posted on May 12, 2018 at 19:44
We used BT139X-600E triac. Opto triac MOC3052 used for triac's control. Load is 230V, 50 Hz LED lamp, current is 30 mA. Current is not very nonlinear - it is short 'pulses' in the maximum of voltage 230 V. The triac must withstand a short-circuit current of 100 A during 10 mS. The problem is that the triac sometimes does not turn on - the reason is most likely a very small current and a large current nonlinearity. We'd like to use BTA12-600BW. Maybe someone can tell what to do in this case?
TIA
Vladimir Naumenkov
2018-05-17 7:47 AM
Hello,
when using an opto-Triac, as soon as the power Triac is at ON-state, there is no more current flowing inside the opto-Triac and then no current flowing inside the power Triac gate anymore.
As a consequence, the power Triac will remain ON only if its A2-A1 current is higher than its proper Holding Current (IH) parameter.
So, with a very low power LOAD like LED 30 mA, a low IH Triac is required (but maybe even not sufficient as the current inside the lamp seems far from being sinusoidal).
ST T1610T-8FP in isolated fullpack package could be tried with Max IH at 25 °C at 15 mA (or BTA12-600TW).
The other source BT139X-600E IH is 45 mA max, typical value 4 mA, 25 °C.
OR (an maybe it is the only solution) a constant gate current must be maintained at the gate terminal.
Maintaining a gate current is requiring an auxiliary power supply linked to an opto-transistor in case isolated control is required like it is in this present case.
Let us know in case of any addition input is required.
Best Regards
2018-05-18 6:30 AM
Dear Mr. Yannick Hague, good day
Thank you.
You reported: '
OR (an maybe it is the only solution) a constant gate current must be maintained at the gate terminal.
Maintaining a gate current is requiring an auxiliary power supply linked to an opto-transistor in case isolated control is required like it is in this present case.'
Please, recommend a practice circuit with an auxiliary supply for maintaining a constant gate current
.TIA
Sincerely,
Vladimir Naumenkov