2021-09-11 10:00 AM
2023-11-02 4:39 PM
In TNxxx - STUSB4500 NVM Description_V1.1.pdf the bit is undefined. However, using the GUI to set and clear the bit and finding the difference in the generated NVM config file I found it is bit 3 of NVM Address 0xE6.
Default value is 0x40 (POWER_ONLY_ABOVE_5V is not active).
Setting the value to 0x48 (bit 3 now set) activates POWER_ONLY_ABOVE_5V. Did test it, works as expected.