cancel
Showing results for 
Search instead for 
Did you mean: 

In the documentation for the STEVAL-CTM009V1 demo board there is a table where the minimum DC bus voltage is listed as 36V, is this really the minimum voltage for the power stage? Why can I not run this board using a motor supply (DC Bus) of 12V ?

sjenn.1
Associate II

I don't need the motor control board, I have my own, I just need the power stage and the capacitor board.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Gigi
ST Employee

Ciao

I', not a big expert of this board but I think it is possible to use it with a DC bus voltage of 12V.

Let's try. Maybe is just a documentation error.

Ciao

Gigi

NBOUM.1
Associate

Hello Sjenn,

I have to pilot a 12V motor with this board but I'm not sure if it's possible with this board,

Did you succeed to pilot it with 12V?

Thanks in advance,

sjenn.1
Associate II

Hi NBOUM.1

In the end we found a different solution so we never tested the board at 12V - sorry! However in my opinion - FWIW - it will work.

I will see if we can get the board up and runnign and test it at 12v.