cancel
Showing results for 
Search instead for 
Did you mean: 

STM3240G EVAL + STEVAL-IHM023V3 didn't work.

phuocnguyenhuu96
Associate III

Hi everyone.

I want to control PMSM using STM3240G and STEVAL-IHM023V3 power board. When I test with Motor Profile Tool, motor working correctly. But when I use Motor Work Bench to generate code and down upto STM3240G, motor didn't work. It's seem like there is no pulse from STM3240G to power board because I do not see the fuse close at first.

Please help me solve problem.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Claire O.
ST Employee

Dear Customer,

We will have a look at your problem.

Can you please indicate the version of MCSDK and CubeMX that you are using?

Thanks a lot,

Claire

Sorry I'm late. Now motor work well. But I just meet a new problem. When I set a high rpm, motor run well but when I set a low rpm, like 100, 200 ... motor didn't work. When I push start button, motor just spin a very little angle and stop. I think this problem caused by PI speed control and modified Kp or Ki but the motor still work.

Please help me solve this issue. Thank so much.

Plus, I use STM3240G EVAL and STEVAL-IHM023V3.

Claire O.
ST Employee

Thanks for your feedback,

I have seen you have open another post for the low speed problem. We will try to answer here...

Claire

Thank you.