cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-ISB68WA not working with standard Qi transmitters

JDupr.2
Associate

"...it works out of the box when placed on a suitable wireless power transmitter." is what it says on page 1 of the user manual. I have several Qi compatible transmitter pads, and the STEVAL-ISB68WA does not power-up with any of them. (D3 does not illuminate and no power is available at the output.)

Is there configuration required to get the STEVAL-ISB68WA to work with a standard Qi charger?

Joe

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
TBurc.1
Associate

STEVAL-ISB68WA not working with standard Qi transmitters

I do have the same issue with the STEVAL-ISB68WA.

Could someone recommend a suitable wireless power transmitter that works with the EVAL Board?

BR Tom

HKhan.3
Associate

Was there a list of compatible Qi chargers?

Hash