cancel
Showing results for 
Search instead for 
Did you mean: 

STEL12H24 RBleed Calculation

OTwin38BoH
Associate

On the STEL12H24, but am not sure about the calculation for Rbleed:

I am designing a 12V system.

RBLEED [kΩ] = VIN / 20 – Rb (min)

Rb would be about 95Ω (from Figure 14 in the datasheet)

That would make Rbleed 12/(20-95) = -160Ω (negative makes no sense)

But according to Table 2, Rbleed is minimum of 560?

Can you clarify this please?

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @OTwin38BoH, to the community!

I am sorry that the formula in the data sheet, section 6.3, might be somewhat misleading. In the formula, the resistances are calculated in kohms, the voltage in volts and the current (the 20) in mA. In addition, there is no bracket around 20 - Rb(min), so VIN/20 must be calculated first.

For your values:

  • VIN = 12V
  • Rb = 95ohms = 0.095kohms

this results in (I have put a bracket around the division for clarity):

Rbleed = (12V/20mA) - 0.095kohms = 0.6kohms - 0.095kohms = 0.515kohms or 515ohms

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

Welcome @OTwin38BoH, to the community!

I am sorry that the formula in the data sheet, section 6.3, might be somewhat misleading. In the formula, the resistances are calculated in kohms, the voltage in volts and the current (the 20) in mA. In addition, there is no bracket around 20 - Rb(min), so VIN/20 must be calculated first.

For your values:

  • VIN = 12V
  • Rb = 95ohms = 0.095kohms

this results in (I have put a bracket around the division for clarity):

Rbleed = (12V/20mA) - 0.095kohms = 0.6kohms - 0.095kohms = 0.515kohms or 515ohms

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thanks for responding. making the datasheet more clear would help a lot.

So the calculated 516 Ohms being less than the specification of 560 Ohms min, I would assume I should still stay above 560, but somewhere in that range?

Kind regards,
Kevin

 

Correct.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.