cancel
Showing results for 
Search instead for 
Did you mean: 

SPV1050 - VMPP range in datasheet?

Bacterius
Associate

Hi,

In the SPV1050 datasheet, in the Electrical characteristics section, the VMPP voltage range is defined as 0.075V to VUVP - 0.1V. I do not understand why VMPP is limited by VUVP. In buck-boost configuration, certainly the input source's maximum power point voltage is potentially above the battery voltage, no? Or does MPPT only work in boost configuration for this IC?

Can you please explain how MPPT operates for a maximum power point voltage above UVP (and potentially even above EOC), in buck-boost configuration?

Thanks in advance!

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0