Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Pulse width Modulation, BEMF and BEMF induced current

Hey guys,I would appreciate your thoughts on this. I have presently implemented 6 PWM schemes to modulate the 2-level 3 phase inverter I am using to control my BLDC motor in a simulation. Those PWM schemes are shown in the figure below I observed tha...

0693W00000GZwewQAD.png

Resolved! Hi, We are planning to use L6491D in our application.

We had the following queries:1.Pins LIN is mentioned as active low.Will the low side PWM output from driver be high when input to LIN pin is low?2.VCC is mentioned to be between 10-20V.But all input pins(SD,HIN,LIN) are operating at 5V level.Is there...

HV Ku.1 by Associate
  • 792 Views
  • 1 replies
  • 0 kudos

Resolved! TORQUE-SPEED RELATIONSHIP?

I have a question, I am presently working with a bldc motor. And I also did a simulation on matlab.So I observed this:1. when I applied a certain load torque (let’s say 0.4Nm), then I give my controller a set point speed (400RPM) the controller is no...

Resolved! Run current limitation

Using SPINFamily Evaluation Tool 3.2, STnucleo-f401re and IHM03A1, I try to drive a 48V-9A motor. In SPINFamily interface, I choosed current mode and tried to set run current to 9A. But an error show up in the interface: "Power dissipation on sense r...

BL1 by Associate II
  • 8468 Views
  • 16 replies
  • 0 kudos

Adding Power Delivery

Hello.1- We want to add USB Power Delivery to an existing converter which can deliver 2x 5.1 V/3A from an unique power stage (isolated converter with one transformer, one regulator IC, etc.).The PD-controller has to meet the following requirements:-N...

FC1 by Associate
  • 2988 Views
  • 4 replies
  • 1 kudos

Avoid back emf on steval-spin3201

Back emf from the motor is entering into other digital causing some issues. How can i avoid/isolate this back emf on STEVAL-spin3201

B.4 by Associate II
  • 868 Views
  • 1 replies
  • 0 kudos

Resolved! How to configure POWERSTEP01 ocd_th in current mode?

Hi,Using IHM03A1, I try to drive a 48V-9A motor. I've set up the POWERSTEP01 driver in current mode, with default registers values, which works nicely but with low torque. Now I want to increase current up to 9A. I've changed IHM03A1 R1 and R2 resist...

BL1 by Associate II
  • 1859 Views
  • 3 replies
  • 0 kudos