cancel
Showing results for 
Search instead for 
Did you mean: 

We use an L6472 with an array 15 of thermal vias under the part to connect to plane layers. Do these need to be solder filled?

CDeWi.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @CDeWi.1​, to the community!

Normally it is not necessary and would also be quite time-consuming/expensive to fill the vias with solder. If the filling is not carried out to a very high and monitored quality, you could face thermal cracking of the vias.

Maybe it would make sense to do a thermal simulation with all thermal parameters?

You could also use thicker copper plating to increase thermal conductivity?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @CDeWi.1​, to the community!

Normally it is not necessary and would also be quite time-consuming/expensive to fill the vias with solder. If the filling is not carried out to a very high and monitored quality, you could face thermal cracking of the vias.

Maybe it would make sense to do a thermal simulation with all thermal parameters?

You could also use thicker copper plating to increase thermal conductivity?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.