cancel
Showing results for 
Search instead for 
Did you mean: 

SPV1040

jramalho9
Associate
Posted on November 02, 2016 at 16:43

We are finishing the design of a solar light using the SPV1040.

Reading the datasheets, application notes and testing the evaluation board STEVAL-ISV006V2, we had a general vision regarding circuit performance.

Anyway there is

two critical questions

that we didn�t find an answer in documentation.

Question 1

We designed all circuit following AN3319 and in page 14 chapter 6 the topic �Input Voltage Partitioning� suggest a resistor from Vmpp-set to PV+ with 1 K ohm (R3 in circuit of page 12).

Why use a low value like 1 Kohm that will sink to much current from solar panel ?

Can we use at least 10K in such resistor ?

What current needs Vmpp-set pin to operate correctly ?

Question 2

Is same topic is not detailed what the relation between solar panel Vmp and the voltage in Vmpp-pin.

Is mentioned that to SPV1040 start operation needs >=0.3V in Vmpp-set pin.

That is the voltage in the Vmpp-set pin when the solar panel reach the Vmp voltage ?

In another words we should start SPV1040 at solar panel Vmp or at a lower voltage ?

If we should start SPV1040 at a lower voltage, than Solar Panel Vmp, what the relation between Solar panel Vmp and SPV1040 start voltage.

To be more clear, if the solar panel have a 2.5V Vmp voltage, we should calculate the both resistors in Vmpp-set pin to have >= 0.3V when solar panel reach 2.5V or before that ?

An answer to the above questions will be helpful to set-up the final values and finish the design.

Thanks in advance.

#spv1040 #steval-isv006v2
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0