2023-07-23 08:45 PM
I am working on SPSB081 power management control IC. I need support in the following points:
1. which revision of data sheet to be followed, because there are some discrepancies in register set(addresses) of revision 2 datasheet.
2. for refreshing the watchdog, TRIG bit should be toggled every time within safe window(7.5 to 12 ms in configuration1, 37.5 to 60ms in configuration2), though i am toggling the TRIG bit of CR1 register for every 50ms, still the NRESET pin is toggling which means reset is happening.
can some one help me in the above points???