2013-04-25 5:56 AM
Hello! I have STEVAL-PCC009V1 and EVAL6470H boards and wondering:
1. What software should I use with STEVAL-PCC009V1?I tried it on Win-XP, after installing drivers it was recognized as Universal Dongle Demo Board. But after starting dSPIN software from here http://www.st.com/web/en/catalog/tools/PF258265 and trying to connect a board, the error appeared that I should connect STEVAL-PCC009V2 board.2. Is there any way to use STEVAL-PCC009V1 board on Win7-64 bit?Thanks, Sergey.2013-04-29 5:18 AM
Hello,
the PCC009V1 board is not compatible with Win7 and it is not supported by the last version of the evaluation software. If you want to test the L6470 using a Win7 machine, you need a PCC009V2 communication board. If you can use the WinXP machine for the device evaluation, please use the attached software. Best Regards ________________ Attachments : dspin_evaluation_tool_1.7.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzFR&d=%2Fa%2F0X0000000bIr%2FcwIc0VYjUAAypmfmtsFY0QOWGofi1sKndijcT88AkFI&asPdf=false2013-04-30 5:34 AM
Thanks a lot!