2013-05-20 5:56 AM
Is there a way to get the identity of the different SPI communicating devices?
I am writing a piece code that can be used by any of our engineers for the L6482, L6472, L6480 or L6470. BUT you have to specify which one you are using. What would be great is at power up, if I could read the part number (or other identifying information) from the part, I could automatically make any necessary firmware adjustments. Thanks, -Pete #motor-control2015-03-09 1:18 AM
2015-03-20 2:59 AM
It's not the solution you look for at first place, but you could do some HW version identification with resistors. Use a resistor with different resistances in divider circuit and based on sampled voltage decide what version of HW you have.
Or you could reserve some Flash area for identifier if you're certain to not erase it...2015-03-20 9:35 AM
Ciao
https://my.st.com/public/STe2ecommunities/motordriver_ics/Lists/Motor%20Driver%20ICs%20and%20Boards
is dedicated to spin family. Ciao GigiWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.