cancel
Showing results for 
Search instead for 
Did you mean: 

Questions regarding the monitoring of ECV voltage by the comparator L99DZ70XP

GreenHand1
Associate

Hello.

I am reading the specification for L99DZ70XP and have some doubts about figure 3 in Section 2.4.1: There are two comparators in the figure used to monitor whether the ECV status is not reached/too high and input the comparison result into the register. I want to know if the registers controlled by these two comparators are bits 0 and 1 in table31 of Section 5.7: ECV voltage too high and ECV voltage not reached? Furthermore, whether the thresholds of the two comparators for determining the ECV voltage are given by programming as described in table31? If the threshold is determined by programming, could you provide or inform us where to download the software routine for reference? If my understanding is wrong, please point out my mistake.

Thank you

0 REPLIES 0