cancel
Showing results for 
Search instead for 
Did you mean: 

PowerSTEP01 - is the ResetDevice command conditional?

CTapp.1
Senior III

I have a PowerSTEP01 that is behaving unexpectedly when I send the ResetDevice command.

If I send it when my system starts then everything is ok when I check the STATUS register.

However, if I send ResetDevice after the motor has been moved (sequence ends with a SoftStop), then the status reports CMD_ERROR. Adding a status check shows that the error was definitely caused by the ResetDevice command - status before is 0xE012 and after is 0xE092.

This does not happen if I issue a HardHiZ before the ResetDevice.

All posts are made in a personal capacity
MISRA C++ Chair
MISRA C WG Member
Director The MISRA Consortium Limited (TMCL)
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0