Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TCPP01-M12 OVP on CC lines

Good morning, I have got a couple quick questions about the TCPP01-M12 chip:Does the OVP protection on CC lines works passively? (no voltage on VCC pin) I am talking about connecting/disconnecting USB plug conditions.What happens when there is perman...

1.png 2.png
withorlo by Associate
  • 920 Views
  • 0 replies
  • 0 kudos

EVLVIPGAN100PD

I've encountered an issue while simulating a schematic in the eDsim software. I attempted to create a schematic resembling the reference design by exporting the schematic of a 100W flyback converter from the online tool of ST eDesign suite. I then ma...

nesrine12 by Associate III
  • 1182 Views
  • 0 replies
  • 0 kudos

Resolved! VNF9Q20F Grounding

From the application schematics of VNF9Q20F, seperating my ground planes for CReg and DVcc but wouldnt DEV_GND (straight from the VNF9Q20F at the bottom) be connected as well instead of to battery ground? Shown as the drawn orange connection. Or both...

DEV_GND.png
TH3221 by Associate III
  • 1937 Views
  • 3 replies
  • 1 kudos

Resolved! Power Path Selector with STMPS2141STR

Hello everyone,  I am designing a PCB and I want a power path selector which can change the source between USB and Battery.Can I do this with STMPS2141STR ? I cannot find a circuit or an application note. This is my design is that correct ? Can someb...

testbenchmark_0-1717484187060.png

Power dissipation of L9960

Hi,we are using L9960 H-Bridge -L9960 for automotive application.Here are the inputs to consider using L9960.ParametersMinTypicalMaxRemarksInput Voltage (UBAT)8. V13.5 V18. VL9960 device will supports 4.5V > < 28VOutput Voltage (Out)7.4 V12.3 V15.75 ...

Amrutha by Associate
  • 1174 Views
  • 2 replies
  • 0 kudos

Resolved! Unable to find diode or cross ref

I am having difficulty locating information regarding some diodes. These diodes are either zener or TVS.Can anyone help me identify it? A link to a cross reference information page would be really helpful. Will be looking to source them for repair pr...

vdc control Diode 2.jpg Snapshot_20240525_1.JPG
Kazit by Associate
  • 2395 Views
  • 2 replies
  • 3 kudos

Stepper motor moves when touched

I'm currently controlling a closed loop stepper motor with an Arduino Uno R3 via the CL86 stepper motor driver. I also connected 2 buttons with pull-down resistors with which I can, for example, rotate the stepper motor by 90 degrees in one direction...

allen22 by Associate
  • 1517 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.