cancel
Showing results for 
Search instead for 
Did you mean: 

Power dissipation calculation for STM32N657X0H3Q

kadam
Associate II

Hello Team,

We are planning to use MCU P/N: STM32N657X0H3Q for our new design. We want to perform thermal simulation. 

Could you please help us for how to calculate power dissipation?

Thanks.

1 ACCEPTED SOLUTION

Accepted Solutions
Bowman32
ST Employee

Why are you referring to Table 4? It is for the STM32H747XI.

If you are using the STM32N657X0H3Q, you should refer to section 6.5 Discovery kit with STM32N657X0H3 MCU.

1) The thermal model of STM32N657X0H3Q

For thermal simulation, you can use 2R thermal model θJB (junction-to-board) and θJC (junction-to-case) in the datasheet.

2) Power estimation 

Power estimation depends on the use case including, PCB size and nbr of layer, copper % ... other component on the board ... and depend also on VDD, Freq.... The power consumption on section 6.5 is presented as test use case example for the discovery board. 

View solution in original post

3 REPLIES 3
mƎALLEm
ST Employee

Hello,

I suggest to refer to the AN5036 "Guidelines for thermal management on STM32 MCUs and MPUs "

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hello,

Could you please help us to understand power dissipation calculation from junction temperature (TJ (°C))
and current consumption? We are referring table "Table 4. STM32H747XI power dissipation versus Tj" in AN5036 application note. Also, we are referring internal Temperature Sensor (TS0 and TS1) for junction temperature estimation.

Thanks,

 
 
 

 

Bowman32
ST Employee

Why are you referring to Table 4? It is for the STM32H747XI.

If you are using the STM32N657X0H3Q, you should refer to section 6.5 Discovery kit with STM32N657X0H3 MCU.

1) The thermal model of STM32N657X0H3Q

For thermal simulation, you can use 2R thermal model θJB (junction-to-board) and θJC (junction-to-case) in the datasheet.

2) Power estimation 

Power estimation depends on the use case including, PCB size and nbr of layer, copper % ... other component on the board ... and depend also on VDD, Freq.... The power consumption on section 6.5 is presented as test use case example for the discovery board. 

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.