cancel
Showing results for 
Search instead for 
Did you mean: 

Partial charge with STBC15 ?

ENGUY
Associate

I can not do the partial charge with STBC15. For example, when the battery is in the BSP state (system is powered by the battery) and the Vbat is 3.8V, if I plug the charger then unplug the charger after some seconds, the Vout is off (0V) ! This is not logic ! Do someone have the same problem ?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0