2018-06-05 1:29 PM
Hello!! I intend to buy the P-Nucleo-IHM001 development kit and I would like to know if there are any free software that I can use to generate the code instead to use IAR.
Does the IAR free license work with the kit ?Regards,Túlio
2018-06-09 7:39 PM
I have
P-Nucleo-IHM002 i
n hand and tried to play with.I tried to use IAR permanent free version (with code size limitation of 32K), it works fine to build the generated code/project.
I use MC SDK 5.1.0 , with STM32Cube 4.25
-Andy