cancel
Showing results for 
Search instead for 
Did you mean: 

Motor control Workbench Monitor via serial error

kissmucus
Associate II
Posted on January 20, 2015 at 14:34

Hi!

I'm trying to use the serial communication between STM workbench and my board.

This is a STM32F3/F4 discovery board, so there are no LCD interface option.

I apply all the ''SystemDriveParams'' files, and the result check in the debug window, all paramaters seems correct.

The Tx and Rx pins uses free I/O ports.

I use the stm motor library v4.0 and Keil 5/4 u vision program.

My prolem:

And I can get that to build and run, but can't get it to establish a serial link.

The Fw start on the controller, and start to measure the DC bus Voltage. No any HW error occurred.

The Baud rates are corrects, the HW connectivity correct, the SERIAL adapter checked whith another serial port.

The STM workbench send the first request 'query about the FW version'

The board results of this query something mix. I checked the UM1052 1 4. chapter but i found the first byte of the answer must be xFF  or xF0,  my first Byte: xFE (both board gets back same result)

My question where i need to check the settings of USART or FW?

I tested two kind of USART port USB/and native, on Win XP and Win7 operating system.

Thanks,

Gabor
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Gigi
ST Employee
Posted on March 20, 2015 at 16:32

I suggest to start to try with the USART examples that is present in the Standard Peripheral Library to verify if the HW is ok.