cancel
Showing results for 
Search instead for 
Did you mean: 

mosfet stp5nk50z

Johan Portier
Associate II
Posted on March 13, 2018 at 18:21

Hello

I am looking for an equivalent of the mosfet stp5nk50z to 220  for a Rolling shutter, thank you

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
T J
Lead
Posted on March 14, 2018 at 12:03

why ?

best to use the right part.

https://www.digikey.com/products/en?keywords=stp5nk50z

 

if you need a better unit we can work on that.

Posted on March 14, 2018 at 17:36

This component is hs and it is no longer available except the Stp5nk50zfp new to electronics, I need to know if it can be mounted instead

Thank you

Posted on March 15, 2018 at 00:44

The Z part is available and the ZFP part is available but not recommmended for new designs.

yes either part can be used,

however on the ZFP part the tab is not conductive.

check if the PCB has the TAB connected to pin 2.

if the PCB has this connection, either part can be used.

Posted on March 15, 2018 at 17:39

If The Z part is available It would be better to choose it but I can't find this reference on the site st.com to buy it

thank you

T J
Lead
Posted on March 15, 2018 at 23:25

I gave you the link above,

it has both parts available.